7/4/2019 2:36 PM | |
Joined: 9/19/2013 Last visit: 4/19/2024 Posts: 21 Rating: (0) |
Dear All, I hope you are all fine and well. I have 3 Function Blocks (22,23,24). FB22 calls FB23 and FB24. The codes inside FB23 and FB24 looks almost the same. When FB22 calls FB23 for example, you see the following parameters:
I "feel" that the block assigns certain "speed" or value to the AO channel according to the state of input flags. I just don't understand where are these values grabbed from as it uses a lot of indirect addressing (DO instruction) and I am not very well at indirect addressing My aim is to convert this into S7, which I think I can do, but I just don't know what are the input values?!! Any help is greatly appreciated. Thanks in advance AttachmentFB.zip (137 Downloads) |
Last edited by: E.Ridy at: 07/04/2019 14:40:58Last edited by: E.Ridy at: 07/04/2019 14:41:18 |
|
Follow us on