11/9/2016 10:19 AM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
Hi Grey, If you have an IPC847D and you want to install PCS7 v6.1 SP4 with a CP1613 A2, it won't work!! You already read my topic... I have solved the problem with this.... What needs to be done is that you must copy a folder from the installation disc of PCS7 v6.1 SP1 to PCS7 v6.1 SP4. It is basically a modified installation of SP4 then. I have this system running in the plant for 1 year now. What I can do for you is upload the modified installation as ISO so you can use it. You have to reinstall Windows XP and then install the modified setup. |
If I could help you, you can use the RATE button. Thank you. |
|
11/9/2016 10:47 AM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928) |
I have done this when I had this problem. They asked Siemens Germany, but they did not know neither. And also it's about v6.1, so it's not supported anymore by Siemens... |
If I could help you, you can use the RATE button. Thank you. |
|
11/10/2016 4:03 PM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Sir Oreca? |
Follow us on