1/2/2008 6:03 AM | |||||
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello; For version 7 of PCS7 there is a supported module calle DP/FF Link, which acts pretty much as a DP/PA link does for Profibus-PA. It is composed of an Anybus DP/FF gateway and a Rosemount3420FIM for FF, and includes a PCS7 library to handle the data from the field. Here are some general descritions of PCS7 with the DP/FF Link shown as part of the configuration: https://pcs.khe.siemens.com/efiles/pcs7/pdf/76/E20001-A214-P280-V1-7600.pdf Here is a link to the DP/FF manual: http://support.automation.siemens.com/WW/view/en/24239833 Here are the part numbers of the Anybus gateway and the Rosemount 3420 FIM units (can't understand why the A&D Mall shows them as Spare Parts, though):
Hope this helps, Daniel Chartier |
||||
1/2/2008 6:40 PM | |
Joined: 1/1/2008 Last visit: 7/3/2022 Posts: 35 Rating: (0) |
Thanks a lot for the detailed info. |
Follow us on