3/23/2016 2:55 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
Sorry, I have a few, but there are official and not allowed to share them...I got virtually b*tch slapped by the moderator for doing that once unintentionally However I found a link with some info: Pharma-food.de I think I may share this....
|
Last edited by: Oreca at: 3/23/2016 3:02:07 PMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/3/2016 8:07 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
Official link: |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/9/2016 3:04 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
PCS7 8.2 Released for delivery! |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/9/2016 6:35 PM | |
Joined: 4/16/2012 Last visit: 10/16/2019 Posts: 2 Rating: (0) |
Old Step7 v5.5 SP4 Upadte9 for Windows7 , not for W10 |
4/9/2016 8:17 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
Correct, only "Clients" are released for Windows 10. I think we'll have to wait for at least SP1 in order to get the rest of the PC stations compatible with Windows 10. Sure there working on it. |
If I could help you, you can use the RATE button. Thank you. |
|
4/9/2016 8:49 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
One thing that disturbes me the most is the fact that PCS7 8.2 seems it does not support the "classic" library anymore (PCS7 7.1 SP3 blocks). So if you want 8.2, you have to re-engineer the plant with APL... Edit:What I mean: A customer who migrated from 6.1 to 8.1 recently without using new functions because its costed too much money is now stuck at 8.1.(looks like it). I told them the time would come that classic would not be supported, but didn't think it was so soon. |
Last edited by: Oreca at: 4/9/2016 8:50:35 PMLast edited by: Oreca at: 4/10/2016 9:28:46 AMIf I could help you, you can use the RATE button. Thank you. |
|
4/10/2016 9:24 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
I've been working with APL for 3 years now..that was not what I meant, but what I meant was that a client has migrated five plant sections from 6.1 to 8.1, without using new functions, because engineering with APL was too much in regard to money. Now it looks like they are stuck at 8.1. Ive told them it was better to use APL and the time would come, but not so soon. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/12/2016 5:08 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
PCS 7 V8.2 - Readme Post-installation of the current version When you install or uninstall an older version of the PCS 7 Library, the PCS 7 Basis Library or the PCS 7 Advanced Process Library after the installation of PCS 7 V8.2 , you must reinstall the latest versions of the PCS 7 Basis Library or the PCS 7 Advanced Process Library. This is necessary in order to guarantee proper functioning of the CFC driver generator. Downloading older versions You can find the libraries of older PCS 7 versions available for download under entry ID 109480136 in the Industry Online Support: https://support.industry.siemens.com/cs/ww/en/view/109480136 |
Last edited by: Thunderstorm at: 4/12/2016 5:09:44 PMLast edited by: Thunderstorm at: 4/12/2016 5:10:42 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
4/12/2016 5:12 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
To my entry above: The page behind the posted link is in progress. It will be released as soon as possible. |
SIMATIC PCS 7 - Overview |
|
4/14/2016 10:07 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
Hi, I had contact with the product manager from Siemens. He said the "classic" library could be used. Why it says "Not available" on the readme, I don't know. Attached is a part of the compatibility list. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to3 thankful Users |
4/15/2016 1:53 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Thank you for your entry. The posted list is an extract of the compatibility list. You find the compatibility tool under the following link: http://www.siemens.com/kompatool Compatibility Tool |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to2 thankful Users |
Follow us on