3/17/2014 3:14 PM | |
Posts: 7 Rating: (0) |
Dear Expert, Can some one tell if PCS7 V8.0 can be installed in windows 7? if possible which type of window 7 Regards! Khobar Woren
|
3/17/2014 3:20 PM | |
Posts: 220 Rating: (11) |
Hi Khobar Woren, yes, you can install PCS 7 V8.0 install on Windows 7. Please look in thecompatibility toolwhich Windows version you need for your PCS 7 Version. |
Last edited by: No Name at: 3/17/2014 3:23 PMLast edited by: No Name at: 3/17/2014 3:22 PMLast edited by: No Name at: 3/17/2014 3:22 PMLast edited by: No Name at: 3/17/2014 3:20 PM |
|
3/17/2014 5:18 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello KHOBAR The following operating systems are supported in PCS 7 V8.0: ● Windows XP Embedded Standard 2009 ● Windows XP Professional SP3 (32Bit) ● Windows Server 2003 SP2 Standard Edition (32Bit) ● Windows Server 2003 R2 SP2 Standard Edition (32Bit) ● Windows 7 Ultimate SP1 (32Bit) ● Windows 7 Ultimate SP1 (64Bit) ● Windows Server 2008 SP2 Standard Edition (32Bit) ● Windows Server 2008 R2 SP1 Standard Edition (64 Bit) Not all configurations are suitable for every operating system. Theattached table shows the relationship of the most common configurations of PCS 7 to the operating systems. Before performing the installation, refer to the product-specific readme files to ensure that the product being installed is suitable for the desired operating system. |
Last edited by: Thunderstorm at: 3/17/2014 6:20 PMLast edited by: Thunderstorm at: 3/17/2014 5:24 PMSIMATIC PCS 7 - Overview |
|
3/17/2015 11:32 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
5/21/2015 11:47 AM | |
Joined: 12/30/2013 Last visit: 10/6/2023 Posts: 7 Rating: (0) |
Hi,
Windows 7 Professional will Support fro PCS7 V8.1 for Client PC as well Engineering Station. |
9/17/2015 10:53 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
New question published by AutoGen_697144 is split to a separate thread with the subject PCS7 OS Client and PCS ES can be installed under Windows 7 Professional. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on