1/5/2008 2:01 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Dear Floyd, Like you say the PPI is for the S7-200 range developed and the MPI is developed for the S7-300 and the S7-400. So thay have the best features for the S7 where they are developed for. Maybe you could do something with the next FAQ: Which HMI components can you connect with S7-200 CPU and what should you watch out for when doing so? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
10/20/2015 10:08 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by pratikbhamare is split to a separate thread with the subject S7-200 PLC has profibus port on cpu or not?. Best regards |
11/4/2015 11:02 AM | |
Joined: 8/21/2014 Last visit: 8/30/2024 Posts: 1006 Rating: (13) |
New question published by pratikbhamare is split to a separate thread with the subject Converting MPI port to PROFIBUS within software. Best regards |
My Forum is the place to personalize your profile, |
|
5/11/2017 1:45 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by NikosNikol is split to a separate thread with the subject Connect pc with plc with profibus cable and adapter. Best regards |
Follow us on