12/17/2014 8:45 AM | |
Posts: 8946 Rating: (999) |
The modules has DIP switches for safety adress? DIP Switches must have the position that is displayed in HW-Konfig. |
12/17/2014 8:54 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, And if no dip-switches, you find the procedure to identify the modules and assign safety address in chapter 2.9; SIMATIC Industrial Software SIMATIC Safety - Configuring and Programming Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to2 thankful Users |
12/17/2014 8:58 AM | |
Joined: 12/16/2014 Last visit: 3/5/2024 Posts: 23 Rating: (1) |
These modules are "new". They don't have any DIP switches. F target address must be assigned through HW cfg, but I can't do that because of that error :( As you can read here: http://w3.siemens.com/mcms/distributed-io/en/ip20-systems/et-200sp/failsafe-io/pages/default.aspx "A special feature of the F-modules of the SIMATIC ET 200SP is the station-wide assignment of F-addresses via the engineering, rather than using the DIP switch (F-address) which needs to be set for each module. |
12/17/2014 9:03 AM | |
Joined: 12/16/2014 Last visit: 3/5/2024 Posts: 23 Rating: (1) |
I read that chapter about 1000 times. When I try to assign the address I get the "The function of this CPU is not supported" error:( |
12/17/2014 9:07 AM | |
Posts: 8946 Rating: (999) |
But you enable "Safety program" in CPU Settings...? |
12/17/2014 10:19 AM | |
Posts: 8946 Rating: (999) |
OK, CPU is new, FW is alsothe latest one. If you try identification of F-Module like sayed in manual, you receive the error message that CPU do not support this function. You may try different Interfaces (MPI/DP/PN) also you may tell us what Version of Step7 and distributed safety. But honestly, I have no idea what the problem is. If nobody else has a good idea, do a Support Request. Perhaps this CPU do not support the new SP - F Modules, I don't know. If you find a solution, please inform us, |
Follow us on