2/22/2020 6:38 PM | |
Posts: 56 Rating: (3) |
hello ixo, maybe the schema attached will help. I need to enter a value between -5 and +35 ° C using TD. depending on the current temperature, I have to decide which controller will be active ideally, a three-state controller would be used. unfortunately there is no such block in LOGO Attachmentreg.pdf (121 Downloads) |
2/22/2020 7:11 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32874 Rating: (4064)
|
I created such a program a few years ago at the special request of a user here in the forum. Maybe it helps you. Attachment3-point stepping controller.zip (121 Downloads) |
This contribution was helpful to1 thankful Users |
2/22/2020 7:47 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
Maybe you are just searching for an easy solution like the program in the attachment. You can setup the difference for starting and stopping as you want. This is a three-state controller for me. Regards, Scorp Attachment3state.zip (140 Downloads) |
This contribution was helpful to1 thankful Users |
2/22/2020 9:18 PM | |
Posts: 56 Rating: (3) |
thanks Scorp, this is what I am looking for. it's very simple - just figure it out :-) |
Follow us on