5/28/2018 12:45 PM | |
Posts: 14 Rating: (0) |
Dear Experts I face a problem during the installation of PCS7 Engineering System on Windows 10 x64bit enterprises. SQL server 2014 SP1 could not installed. |
5/28/2018 1:07 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Windows 10 enterprise is not released, you need Windows 10 LTSB 2015 in case you want to use Windows 10. See the following topic. All kind of problems can arise when new updates are installed for Windows 10. Topic Last week I updated my Windows 10 and Windows decided to uninstall a display link driver, because it was not compatible anymore with the new Windows version. Thanks Microsoft for creating problems! That's why you need LTSB which means you will not receive any updates that prevent PCS7 from working. |
Last edited by: Oreca at: 5/28/2018 1:26:06 PMIf I could help you, you can use the RATE button. Thank you. |
|
5/28/2018 1:33 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi Malix, please check if you have installed the feature .NET framework 3.5. See the notes from Microsoft: Regards |
Follow us on