1/22/2015 7:23 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Have a look here: Which version of STEP 7 Micro/WIN or S7-200 PC Access is compatible with which version of MS Windows and read the FAQ about your PC adapter, I think you have a problem there: Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5 Regards, Marcjan |
Problem solved? |
|
1/23/2015 7:53 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Microwin works as far as i knowwith all windows 7 versions, The problem you have is in my opinion related to your PC/PG adapter and it's drivers. Can you show us a printscreen with all interfaces installed? Please note you have a PC adapter not a PC/ PPI cable. Is Microwin the only simatic program installed or do you have also Step 7 V5.x ? Regards, Marcjan Attachmentpc adapter.pdf (1466 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
10/19/2015 1:25 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22230 Rating: (2980) |
Hello, in the first listbox (S7Online...) is here a entry for MicroWin? Regards Chistoph |
10/2/2020 11:57 AM | |
Posts: 1 Rating: (0) |
how to do this? |
10/2/2020 1:54 PM | |
Joined: 9/21/2012 Last visit: 4/26/2024 Posts: 3923 Rating: (444) |
How to do what? |
This contribution was helpful to1 thankful Users |
Follow us on