3/7/2019 8:07 PM | |
Joined: 2/16/2019 Last visit: 9/29/2023 Posts: 25 Rating: (0) |
I am trying to write a program that uses an input (pulse switch) and a flag to switch a pulse relay. The flag is used in a web program. The problem is that the flag should also act as a pulse switch. Is this possible and if so how. Is there another solution on how to combine the control of a relay from the logo program and a web interface? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/8/2019 6:46:54 AMNew subject after splitting |
|
3/7/2019 8:28 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33835 Rating: (4205)
|
Hello brunodecoen, in attachment are two possible solutions. |
3/7/2019 8:42 PM | |
Joined: 2/16/2019 Last visit: 9/29/2023 Posts: 25 Rating: (0) |
I am writing the web program with the Logo! Web Editor. |
3/7/2019 8:53 PM | |
Joined: 2/16/2019 Last visit: 9/29/2023 Posts: 25 Rating: (0) |
Thank you very much. It seems to do the trick. |
This contribution was helpful to1 thankful Users |
3/7/2019 8:59 PM | |
Joined: 2/16/2019 Last visit: 9/29/2023 Posts: 25 Rating: (0) |
I got the first option working. The seconds not just yet. How do you control the network input in the Web editor? |
3/7/2019 9:01 PM | |
Joined: 2/16/2019 Last visit: 9/29/2023 Posts: 25 Rating: (0) |
Never mind, i figured it out. I have got both methods working. Thank you very much! |
Follow us on