2/15/2017 11:03 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
I have times a simple UDF created and integrated into a program. At the function I can not find any misconduct. |
2/15/2017 11:43 AM | |
Posts: 5 Rating: (0) |
Weird, I cannot get it to work. Maybe I make a conceptional error. I attached a dummy I just clicked together. It contains an analog threshold that should have its output on between values of 125-250. It works fine in simulation (sensor type set to 4..20 mA). But when I include it in the final circuit diagram, the trigger is not working anymore. The hardware is set to have AI1 be a 4..20 mA sensor. cheers --bruno Attachmentdummy.zip (77 Downloads) |
2/15/2017 2:56 PM | |
Posts: 5 Rating: (0) |
The sensor ts in the range of 4..20 mA. Ultimately it is measuring pressures between 0 and 400 bar. I am basically trying to extract some duplication out of an existing Logo program (that is working fine) into UDFs for better reuse. When I run my the final Diagram, nothing works in simulation, I cannot get it to trigger at the desired value. Running just the UDF (after manually resetting the sensor type to 4..20 mA), the UDF simulation is working fine. I attached some screenshots of my problem. thanks again! cheers --bruno Attachmentscreens.zip (108 Downloads) |
2/16/2017 9:30 AM | |
Posts: 5 Rating: (0) |
Thanks a bunch! cheers --bruno |
This contribution was helpful to1 thankful Users |
Follow us on