7/22/2019 2:27 PM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Please also see the attached acreenshots. We have a machine that is controlled by an old S5 PLC I am trying to find out which HW I need to buy to to replace it. I do however realize that I need a base unit for each of the I/O modules (maybe for the CPU also?) but which base unit is correct for which I/O module and how do I see that? Also - how many I/O modules can be connected to the CPU unit directly and how many I/O "stations" (ET 200 remote I/O racks) do I need to include? 1 pc SIMATIC DP, CPU 1510SP F-1 PN 6ES7510-1SJ01-0AB0 12 pcs ET 200SP, digital input module 6ES7131-6BF00-0CA0 16 pcs ET 200SP, digital output module 6ES7132-6BD20-0BA0 4 pcs ET 200SP, analog output module 6ES7135-6FB00-0BA1 3 pcs ET 200SP, F-DI 8x 6ES7136-6BA00-0CA0 1 pc ET 200SP, F-DQ 8X 6ES7136-6DC00-0CA0 AttachmentS5 PLC.zip (270 Downloads) |
7/22/2019 2:38 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
Have a look on the SINAMTIC Selecton Tool. Designing your PLC is easier with it. You may export the HW configuration to TIA Portal. Online: www.siemens.com/tia-selection-tool Windows: http://www.siemens.com/tia-selection-tool-standalone |
|
|
This contribution was helpful to1 thankful Users |
7/22/2019 3:02 PM | |
Joined: 9/30/2016 Last visit: 5/13/2024 Posts: 911 Rating: (6) |
Thank you for answering miami, I will give the selection tool a try.and see if I can figure it out. |
7/22/2019 3:43 PM | |
Joined: 7/9/2015 Last visit: 5/13/2024 Posts: 3830 Rating: (557)
|
Hi, normally this informations are visible in the technical data of modul i.e. there you will find information "Usable BaseUnits". also check this: Which Base Units can you use for the IO modules of the ET 200SP?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on