9/10/2014 7:06 PM | |
Posts: 9 Rating: (0) |
Thank you very much for your answer. Unfortunately I`m just learning WinCC and also I`m writing my master`s thesis... In my thesis I have to test the rate of saving variables to CAS. So this is not a large installation (only a few tags – INTERNAL variables, there aren`t external tags and PLC). I need a simple solution that will allow me to carry out the relevant tests. So I think, that I need WinCC CAS, WinCC Server and WinCC Client (is it necessary?), no ES Station. I tried do this 5 steps, which are described in WCASInformationSystem (pages 20-31), but of course it doesn`t work... I create in SIMATIC NCM Manager 3 SIMATIC PC Stations: one with CAS Appl., one with WinCC Appl. and one with Client Appl. But I can`t "Assing OS Server". Could you explain me, how should it work? Maybe something isn`t described in manual... ;( I tried also create only multi-user project and the client can activate or deactivate project on server, but I can`t open this project on client. Every time I get this error: "Invalid command line parameters! Try one of the following: MCP.EXE /R (Registering) MCP.EXE /R /T (Extend Registering) MCP.EXE /L:<LCID> (language)" AttachmentWCASInformationSystem_en-US.pdf (232 Downloads) |
9/12/2014 10:15 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
Follow up question published by sarula_91is split to a separate thread with the subject problem while trying to download project between two SIMATIC PC Stations in SIMATIC NCM Manager. Best regards Min_Moderator |
Follow us on