6/15/2013 10:30 AM | |
Posts: 5 Rating: (0) |
I've answered my own question after some searching on the Siemens website. I have attached the Siemens instructions that cover it... There is no need to write the flag state to VM memory on the server, as the client can read the state of the flags on the server directly. It can also read the input and output state. I hope this helps anybody else trying to work out how to get started with LOGO networking. Russ Attachment06_Comunicação Mestre-mestre.pdf (502 Downloads) |
This contribution was helpful to1 thankful Users |
5/9/2016 10:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Bill1777 is split to a separate thread with the subject Change of addresses of Inputs, outputs and flags in VM memory with LOGO! 8. Best regards |
Follow us on