8/9/2017 3:24 PM | |
Joined: 1/3/2013 Last visit: 9/12/2024 Posts: 40 Rating: (3) |
Dear experts, I have an application where I need to use the CP 1242-7 GPRS V2 connected to a S7-1214C PLC to send messages or receive commands Being my first time working with GSM/GPRS networks I looked for available application examples. I found Signaling and Switching via SMS with S7-1200 and CP 1242-7 GPRS V2 (Set 32) perfect to check and better understand how setup works. I modified the project found in the application example to fit my needs in terms of GSM numbers and security.
Right after I activate the functionality of SetGet from the HMI I got the following error code: 00118088 and of course no SMS with the already defined commands was identified in the application. Still, I found that I could see the correct SMS messages in the online&diagnostics of the 1242-7 GPRS v2. Please check the attached picture. I looked in the application example document for the corresponding error code. It seems that TRCV_C function is responsible. Took a look in TIA Portal help for this function error codes and found that there is an issue with the fact that receive area is to small or that the value of the LEN parameter is larger than the received area set in the Data parameter I also activate the RcvSms functionality, still the same error and sometimes got another error code: 0011_80C5. This error code seems to be related to the fact that the remote partner has terminated the connection. If you have any advice on how to solve this issue please be kind and share it. Best regards, Mircea. |
9/25/2017 1:16 PM | |
Posts: 1 Rating: (0) |
Hello, I have exactly same problem now. Do you have any solution, or you still waiting for some suggestion. Thank you very much for info. |
Follow us on