11/30/2012 12:48 PM | |
Joined: 9/27/2006 Last visit: 5/5/2024 Posts: 12257 Rating: (2666) |
Hello aliuta; SEW Movidrive provide excellent support, either in documents or over the phone, when it comes to connect a Movidrive to a S7 PLC. Have a look at the following documentation provided by SEW: Profibus Manual with details on parameters (in Movidrive) and configuration (in S7 HWConfig): Manual Fieldbus Interface DFP21B PROFIBUS DP - Sample programs for S7 PLCs: Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on