10/16/2013 12:55 PM | |
Posts: 1 Rating:
|
HI.. I want to establish communication between TDC CPU & S7 416 CPU over ETHERNET. I have attached hardware configuration of both systems. Kindly let me know what settings has to be done in Netpro and what has to be done in TDC. Regards, Bhushan Bapat AttachmentHardware Config.zip (266 Downloads) |
10/16/2013 1:51 PM | |
Joined: 8/25/2006 Last visit: 8/15/2024 Posts: 2208 Rating:
|
Hello. For S7-416: 1. Create Ethernet network 2. In Netpro add Other station (this is TDC) with the IP inside the same subnet 3. For CPU416 in Netpro add a new connection (TCP or UDP) with Other station, one for send and one for receive. If use TCP set active for sending. Set different local/remote ports for each connection 4. Create S7-program For TDC: 1. In HWConfig set IP address as you use for Other station 2. Create CFC-program. Manual for configuring IE communication ishere.
|
This contribution was helpful to
1 thankful Users |
Follow us on