3/20/2018 8:44 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Krishna; Two-speed motors are wound in a very distinct fashion compared to squirrel-cage motors, fro example.. Changing from one speed to another means that you must connect and disconnect the leads and the windings on the fly,which requires high-power electronics and the use of pushbutton to caommand them. See these examples: Theory: Two Speed Dahlender Winding Types - ELK Motor Youtube: two speed motor starter connection and working function animation Hope this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 3/21/2018 8:48:12 AMInserted video. |
|
This contribution was helpful to1 thankful Users |
Follow us on