5/31/2017 3:55 PM | |
Posts: 14 Rating: (9) |
Hi there, I am trying to access a SQLite3 database in an Express application. To establish a connection between SQLite3 and Express I tried to install the driver via "npm install sqlite3", but all I get is this:
Has anyone some help to offer? Is it really necessary to install that driver? I'm afraid I'm pretty new at working with the IOT, node.js, Express and SQlite3. Greetings! |
6/1/2017 8:56 AM | |
Posts: 14 Rating: (9) |
Thank you, but I know that SQlite3 is already installed, that's why I didn't use
I wanted to create a SQLite3 database via node.js with this example code I found on the internet:
But if I try to run it, it complains that "node_sqlite3.node" is missing so I tried to install it via npm as recommended here. But it produces the error I copied in my first post. I also get this error if I try
and I really don't know what to make of this error.
|
9/19/2017 3:27 PM | |
Posts: 52 Rating: (2) |
As I can only upload only Screenshot at a time I attached the second part of the errors here: |
Follow us on