7/18/2018 12:37 PM | |
Joined: 6/26/2016 Last visit: 11/15/2023 Posts: 5 Rating: (0) |
hello i have profibus network (i\o units , vfd (micromaster)) and i put OB 80,81,.... to solve stop cup problem but if the i\o remove the CPU still run and S.F led goes run light but if you remove micomaster the CPU goes stop . now how i can still cpu run if remove micromaster ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/18/2018 3:33:17 PMNew subject after splitting |
|
7/19/2018 5:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
In PLC hardware project you need to remove micromaster & needs to modify PLC logic where ever MM signal interlocks are written/read. |
Follow us on