10/17/2018 5:10 PM | |
Joined: 4/7/2016 Last visit: 4/14/2024 Posts: 8 Rating: (0) |
Hi, thanks for the answer. I have tested the VDF in OLTM with a flux demand in 0.8 and the Flux Ds graph oscilatte so much. The drive is going to Over voltage fault. This is the same behavior with motor connected in V/Hz control. Thanks AttachmentT13_Parameter Dump 10-16-2018 2-11 - Copy.txt (547 Downloads) |
10/17/2018 6:04 PM | |
Joined: 4/7/2016 Last visit: 4/14/2024 Posts: 8 Rating: (0) |
Here is the graph in OLTM. |
Follow us on