12/10/2017 7:31 PM | |
Posts: 37 Rating: (3) |
Hi all, I am looking for a schematic of the IOT2040, specifically how are all the IO pins connected to which chips and pins. For the Intel Galileo Gen 2 there is the following information, but for the IOT2000 it is different: https://www.intel.com/content/dam/support/us/en/documents/galileo/sb/galileo_fabh_schem_120514.pdf Without that information it is impossible to get background information which is needed to adapt kernel configuration and drivers. For example how to get the IRQs working, which pins are directly connected to the internal GPIOs of the CPU and which are routed via the i2c bus, which pins are multiplexed, how to get fast SPI (with CS) working. Michael |
12/11/2017 9:58 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi Michael, there is a Intel information about GPIO mapping. You can find it here: https://communities.intel.com/thread/55920 This information is valid for the IOT200 as well. Does this help? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
12/12/2017 7:06 PM | |
Posts: 37 Rating: (3) |
Hi bergmanu, thanks, that table answers a lot of questions! Michael |
This contribution was helpful to1 thankful Users |
1/10/2018 10:02 AM | |
Joined: 8/21/2014 Last visit: 4/24/2024 Posts: 951 Rating: (13) |
New question published by kurtl is split to a separate thread with the subject SIMATIC IOT2000 I/O Shield on IOT2040 questions. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on