10/6/2016 10:42 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
We provide an SD-Card Example Image. If you want to create your own image, you can do this as well. Required for this is a Linux based building environment. The following builds have been successfully tested on Debian 8 and OpenSuse 13.2, but other recent distros are expected to work as well. There are two build instructions (README.md) to do so on GitHub (https://github.com/siemens/meta-iot2000): At first there is the “meta-iot2000-bsp”, which is the official board support package. It allows building standard Yocto images which will contain the required kernel, configurations and tools and will emit a bootable SD card image. Based on this there is the “meta-iot2000-example”. This Yocto layer builds on top of “meta-iot2000-bsp”, providing an exemplary image with additional tools and services to exploit features of the IOT2000 conveniently. This layer shall only be considered as a starting point for own developments. It is not configured to provide product-grade maturity and security. If you follow the instruction for building the “meta-iot2000-example” layer, you will get exactly the SD-Card Example Image provided by us. |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
6/26/2017 8:58 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating:
|
FYI: Santiago's report is now tracked at https://github.com/siemens/meta-iot2000/issues/51. |
7/26/2017 11:56 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating:
|
Please see https://support.industry.siemens.com/tf/ww/en/posts/building-latest-sd-card-image-simplified-process-available/171736/?page=0&pageSize=10 for an update on & simplification of the build procedure. |
Follow us on