7/26/2018 1:00 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please refer SIMOVERT MASTERDRIVES, MOTION CONTROL, COMPENDIUM CUVP = Control unit vector control compact PLUS. It is main control electronics board. (page 308) ASIC (Chip) = SBM type sensor board code number 112 for SIMOVERT MC technology function suitable for encoder ERN1397, ECN1313, EQN1325, SSI . (page 845) HTH. |
Last edited by: PISCEAN 2010 at: 7/26/2018 1:02:44 PMLast edited by: Jen_Moderator at: 7/26/2018 2:17:22 PMOptimized link. |
|
7/26/2018 1:36 PM | |
Joined: 10/11/2006 Last visit: 4/18/2024 Posts: 5818 Rating: (787)
|
Hello, I think there are two options
For case two the MLFB should be provided. For case one the question would be, why this information is needed. Note: SBM may not be asked, as it is not compatible to CUVP
|
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on