9/26/2018 4:23 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi community, as you know we provide an Example Image for the IOT2000. As you know as well, using it "as it is" is not that secure, for instance there is only the root account without password by default. For solving this and other things, that might affect security, I prepared a document with the most usual settings you can do to improve the security of the device. Keep in mind that these settings are only examples you can do and of course there is no claim to completeness (I think there is no completeness at all for the security topic). See it as little guidance and if you have other tips, please share them with us Best regards! AttachmentSecuritySettings_for_IOT2000.pdf (1726 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to4 thankful Users |
12/13/2018 3:22 AM | |
Joined: 5/4/2011 Last visit: 4/19/2023 Posts: 16 Rating: (2) |
There is no 100% security. |
This contribution was helpful to1 thankful Users |
12/14/2018 5:13 PM | |
Posts: 439 Rating: (108) |
But you can improve it the best you can. |
Follow us on