10/30/2018 2:25 AM | |
Posts: 4 Rating: (0) |
Dear expert, I would like to make a follow-up question. The manuals that you mentioned provide very few details about the encoder and although the output pins are provided, I can not figure out what are their functions and what is the communication used. Is there any other document with a more detailed explanation for each encoder option? I am interested in encoders without the DRIVE-CLiQ. I saw that the absolute encoder has A, A*,B, and B* signals, are those incremental signals? will they be available if I order an absolute encoder? For an incremental encoder, I would like to know for example if the signals at the terminals of the incremental encoder sin/cos 1Vpp are analog or digital signals. Is there any option which provides digital signals for an incremental encoder? I would really appreciate any help. I have already called Siemens many times and they just keep transferring my call which is extremely frustrating. I appreciate any help. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2018 11:39:43 AMNew subject after splitting |
|
10/30/2018 11:41 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
Closed cause question posted twice. The second thread with the subject Encoder options for 1FK7 without DRIVE-CLiQ is published within the conference SIMOTICS / MOTION-CONNECT.
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on