4/6/2019 1:08 PM | |
Posts: 6 Rating: (0) |
Dear, I would like to know if the Wincc is compatible with the OMRON PLCs. |
4/6/2019 3:10 PM | |
Joined: 9/27/2006 Last visit: 9/25/2024 Posts: 12283 Rating: (2685) |
Hello; "The" WinCC comes in various packages, associated with different software environments; which one do you plan to use? The following manual accompanies WinCC v15.1 (TIA Portal) and discusses Host Link connections with an Omron PLC: SIMATIC WinCC WinCC Engineering V15.1 – Communication https://support.industry.siemens.com/cs/ww/en/view/109755215/115228705675 If you are using WinCC v7,5, there is no longer an Omron driver available in the software. However, you can always connect to Host Link through the WinCC OPC channel, provided you can have a OPC server for the PLC. Hope this helps, Daniel Chartier |
Follow us on