10/16/2018 2:07 PM | |
Joined: 4/13/2015 Last visit: 5/9/2024 Posts: 8 Rating: (0) |
How should I start to get working the IOT2040 + Siemens RFID Card Reader? I connected the RFID to the IOT2040 serial port and I'm trying to realize a demo application in node-red. Should I just find out how to interrogate the RFID reader, and send some telegrams through the serial port? I hope to to understand which telegrams to send from monitoring the S7-1500 FBs. Before waisting my time, I would like to know which is the advised method. Wouter ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/17/2018 10:12:40 AMNew subject after splitting |
|
10/17/2018 10:10 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I don't know how DJ_1 managed to set up a serial communication with the RF1060R, since there is no documentation on the communication protocol of this device. The only example code I know of is in C#, which you could only run on the IOT if you have Mono installed. But the problem is that the driver library is precompiled for Windows 32/64Bit. To be honest I would suggest working with a different RFID Reader like the RFID-RC522. There is a lot of documentation on this reader and it is also capable of reading MiFare company badges. Kind regards! |
Last edited by: Fe_lipe at: 10/17/2018 10:15:03 AMAdded Hyperlink |
|
Follow us on