3/13/2018 2:00 AM | |
Posts: 4 Rating: (0) |
Hi All, I am working on a project which used TIA V13 SP1 (PLC: S7-1200) , It was compiling and downloading to the PLC very well when I was working through one VM. But when I connect to another VM, as soon as I make a very small change, such as adding a Tag in one DB, it cannot be complied and download any more. I see “An internal consistency error has occurred” and it ask to compile all of the other FBs and DBs and OBs which already being compiled correctly before. And even by compiling the whole project or even deleting the changes, the error remains. Solutions such as rebooting the PC didn’t work in my case. and date and Time of both VMs are the same. I will appreciate if anyone can help me. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/15/2018 9:25:02 AMNew subject after splitting |
|
3/15/2018 7:21 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by #dP is split to a separate thread with the subject RIP Stephen Hawking . Best regards |
My Forum is the place to personalize your profile, |
|
3/18/2018 8:09 PM | |
Posts: 4 Rating: (0) |
Hello, Thank you for the suggestions and recommendations. The problem solved by installing TIA V13 SP1 Update 9 |
This contribution was helpful to1 thankful Users |
Follow us on