4/21/2019 9:10 PM | |
Posts: 2 Rating: (0) |
Hello Everyone, I have been trying to get a Put to work from a 300 to 1500 and I have no success. I can have a Put or a Get from 1500 to 300, and that works. I have a 1518 and a 319. 1518: 53.11.168.244 319: 53.11.168.243 They are plugged to the same switch. I followed this instructions, but no luck https://support.industry.siemens.com/cs/ww/en/view/92269951 I have error 1 with status 1. Thank you for the help Roberto Mello |
Last edited by: Jen_Moderator at: 4/22/2019 1:12:20 PMOptimized link. |
|
4/23/2019 10:07 AM | |
Posts: 1368 Rating: (126) |
Hello RoboMello, here you fnd a FAQ for S7-1500 https://support.industry.siemens.com/cs/ww/en/view/82212115 Please note: You must allow the PUT/GET communication in S7-1500 (HW-Config > Properties). Otherwise, you are not able to get/put data into or from S7-1500. |
5/2/2019 3:52 PM | |
Joined: 8/3/2009 Last visit: 4/18/2024 Posts: 12813 Rating: (1634) |
Hello RoboMello I think this one is suitable for you, its a S71200 but the procedure should be the same: https://support.industry.siemens.com/cs/de/en/view/92269951 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on