4/18/2019 4:33 PM | |
Joined: 8/10/2017 Last visit: 5/25/2023 Posts: 22 Rating: (0) |
Hi , I need to migrate a project from Step 7 v5.6 which has an HMI MP377 on WinCC 2008 flexible to TIA v15. I understand the MP377 is not compatible with TIA v15. What will be the best solution? -Is there any HMI on WinccFlexible 2008 that I can use to replace the MP377 and than migrate the project? Thansk ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/19/2019 9:58:43 PMNew subject after splitting |
|
4/18/2019 4:46 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, have you already seen this: https://support.industry.siemens.com/cs/us/en/view/109754931 |
Last edited by: Jen_Moderator at: 4/20/2019 11:23:26 AMOptimized link. |
|
4/18/2019 5:09 PM | |
Joined: 8/10/2017 Last visit: 5/25/2023 Posts: 22 Rating: (0) |
Hi, Thanks, for your answer . I had a look at it yes. But maybe I'm misunderstanding some of it .. If old devices are in the project, you have to switch these devices over to a current device (Comfort Panels, Basic Panel 2nd Gen or similar). Instructions for this are available in the manual "SIMATIC STEP 7 Basic/Professional V15 and SIMATIC WinCC V15" (entry id109755202) in the chapter "Visualizing processes -> Using global functions -> Replacing devices". Does that mean I need to replace it on WinCC 2008 Flexible or TIA v15 ? Because, when I try to replace it (MP377) on Wincc I can't find any of HMI's specified above.
|
Follow us on