Default Header
(header konnte nicht geladen werden)
5/8/2017 11:17 AM | |
Posts: 3 Rating:
|
Dear all, I have 1600 KW Simadyn D drive it was running with out load but when drive started with load it was dispalaying alarm ( " over current torque direction 1 " & " over current rotor circuit " ) and motor not running " slip ring motor , 11kv power supply " . ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/9/2017 1:10:25 PMNew subject after splitting |
|
5/16/2017 2:54 PM | |
Posts: 3 Rating:
|
This is alarm signal of my Drive |
5/16/2017 3:19 PM | |
Posts: 3 Rating:
|
at Start time " I set " reach to more than 1000 Amp. . the DRIVE is SEMOVERT |
Follow us on