6/20/2018 7:47 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
http://www.modbus.org/docs/Modbus_Application_Protocol_V1_1b.pdf see page 15. start adress 0x0000-0xFFFF frantaM AttachmentModbus_Application_Protocol_V1_1b.pdf (214 Downloads) |
Last edited by: Jen_Moderator at: 6/21/2018 9:42:02 AMAdded file as an attachment. |
|
6/20/2018 7:52 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
Take a look at attachment.
AttachmentModbus Implementierungstabelle (Scorp).pdf (181 Downloads) |
6/20/2018 8:00 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
yes this is a problem when VW0 is maped as HR1 bus modbus start to 0 correctly would be vw0 = HR0 FrantaM |
6/20/2018 8:15 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
An excerpt from the online help. VW0 = HR1 AttachmentLOGO! 8 Soft Comfort Online-help 2017_11 V8.2 page 60.pdf (192 Downloads) |
6/20/2018 8:54 PM | |
Joined: 2/12/2016 Last visit: 1/8/2024 Posts: 69 Rating: (9) |
yes but all device thirty part use modbus starting from zero. only logo start from one |
6/20/2018 9:07 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
May be correct, but helps not by the LOGO!. And wehave to follow the rules for working with the LOGO!. |
Follow us on