4/24/2016 11:34 AM | |
Posts: 5 Rating:
|
Hello, We have a use to Generator excitation system THYRIPOL . We must change generator under excitation limiter for reactive test completed. I found the parameters to be changed. How do I connect the computer to the T400 technology card ? How do I download the program in my computer 's T400 available ? Can you help me ? Thank you in advance for your help Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/25/2016 9:48:23 AMNew subject after splitting |
|
4/24/2016 1:03 PM | |
Joined: 8/25/2006 Last visit: 9/17/2025 Posts: 2218 Rating:
|
Hello. What order number of your T400?
If you have CFC-program for T400, then you can download it via RS232. If your T400 is with standard program you can download/upload parameters backup using DriveMonitor.
|
This contribution was helpful to
2 thankful Users |
4/24/2016 3:24 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello You will need a connecting cable as described in Section 3.7.1.2. Connecting cable to the PC of attached T400 Brief Description Link for : T400 - Detailed User Manual Hope this helps Cheers Navnag AttachmentT400_Brief_Description.pdf (1467 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
4/25/2016 2:49 PM | |
Posts: 5 Rating:
|
I must change generator under excitation limiter for reactive test completed. I need to change two parameters T400 card. Step vay step 1- T400 card, I connect a PC with the installed base of CFC and D7-SYS software 2- I update the program on my desktop, connecting the T400 card 3-then I'll change two parameters 4-After I download the program in T400 programs on the computer is attached I will change when you open the program parameters in section Begrenzungen Names of parameters : L131, L132, L133, L134, L135, I ask you: Can I change this way. Is any problem happens ? Thank you for helps Best Regards AttachmentSey_2_K1.zip (1018 Downloads) |
Follow us on