11/12/2018 2:26 PM | |
Posts: 10 Rating: (0) |
[snip] in end user i will using mobile phone or laptop to read the data by php file, which is connected with wireless router (ping are working good) and mobile phone can read database but blank table. thanks before. Best Regards, Insan (Indonesia) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/13/2018 9:48:41 AMNew subject after splitting. Division of questions into separate topics. |
|
11/12/2018 2:32 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379) |
Hi, that depends on the environment you are using. With node-red it is more easy than with C/C++. If you are using node-red you can use for example the s7 node to read out data from a PLC. In this case you just have to alloow PUT/GET communication in TIA Portal and use a non-optimized DB. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
11/13/2018 6:51 AM | |
Posts: 10 Rating: (0) |
hi, i have a PUT communication on tia portal, on "SD_1" connected to mydb. But i dont know how to connect "ADDR_1", because this is address of IOT, can you give me solution?... thanks, Best Regards, |
11/13/2018 3:11 PM | |
Joined: 8/3/2009 Last visit: 9/24/2024 Posts: 13764 Rating: (1738) |
Hello insanah At Siemens you will only find the SIemens internal solutions like: https://support.industry.siemens.com/cs/ww/en/view/109746168 Or you use a common protocol like OPC UA. With S71500 V2.6 and V15.1 you can use it as OPC UA Server or OPC UA Client Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on