12/4/2015 8:41 AM | |
Posts: 14 Rating:
|
Hello guys, Hardware I am using is CPU 1214c, incremental encoder 1024 PPR. I can't receive this 1024 pulses when I make 1 revolution by hand. The digit which I receive for 1 revolution is between 10 and 30 I do everything by the books, however my HSC of CPU 1214C in my oppinion is counting as a regular counter, not High speed counter. I complete hardware setups: First Enabling HSC1, then choosing single phase, type is counting, count up, I0.0, I am not using any interrupts, because I am just testing. In the program I have tried to call the HSC in OB1 and reading ID1000, also I tried to do this in FC still no success. Please, let me know if you know how to read correctly 1024 pulses per revolution. Best regards, ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/4/2015 1:07:39 PMNew subject after splitting |
|
12/3/2016 12:19 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by ahmad_hf is split to a separate thread with the subject 1200 CPU loss encoder pulse when the frequency is about 500Hz. Best regards |
Follow us on