8/5/2016 11:11 AM | |
Posts: 2 Rating:
|
Hi , can we integrate ST-30 s7-200 smart PLC with Kepware OPC Server? which hardware & software required for it ? please help me. |
8/5/2016 2:29 PM | |
Joined: 9/27/2006 Last visit: 8/15/2024 Posts: 12277 Rating:
|
Hello tej; The S7-200 Smart PLCs are a development of the origninal s7-200 CPUs for the Indian market, and there is little information available for us on these units. Here is a catalog that could help answer your questions: In the catalog it is mentionned that the S7-200 Smart CPUs have an integrated Ethernet port that supports S7 protocols. Kepware supports S7 protocols over TCP/IP with many families of s7 PLCs: A small paragraph in the catalog suggests that a Siemens OPC server (PC Access) will connect to the S7-200 Smart over TCP/IP; I would be enclined to believe that the connection to the Kepware OPC should be established without problem. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
12/16/2016 12:15 PM | |
Posts: 4 Rating:
|
Dear All, Please refer tech-note. We have successfully tested this yesterday. Please rate if you find it useful. AttachmentKepware With S7-200 Smart.zip (1572 Downloads) |
Last edited by: Siemens sumit at: 12/16/2016 12:16:22 PM |
|
This contribution was helpful to
8 thankful Users |
3/12/2017 6:31 PM | |
Posts: 4 Rating:
|
You dont use MW & MD tags in S7-200. Read Addressing manual for S7-200 first. |
9/19/2017 7:37 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
New question published by Prakashni Singh is split to a separate thread with the subject Communication between s7-200 smart with s7-200 smart plc using get/put Ethernet . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on