(7)| 12/29/2019 10:00 PM | |
|
Joined: 9/23/2005 Last visit: 1/20/2026 Posts: 4450 Rating:
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. As from the TIA V16, there was the introduction of the WinCC Unified. This is an engineering platform for HMI Comfort Unified and for WinCC Unified PC. It brings many news regarding the WinCC Advanced / WinCC Professional. One of the news of WinCC Unified is the support of SVG graphic elements. They are scalable and compliant with HTML5 technology. TIPs:
The attached project show some example of SVG files. Project (.zap16 ziped as .zip)
AttachmentSVG.zip (4135 Downloads) |
Last edited by: Denilson Pegaia at: 12/30/2019 10:37:09Last edited by: Denilson Pegaia at: 12/30/2019 10:39:24Denilson Pegaia |
|
This contribution was helpful to
|
|
| 2/27/2020 4:38 PM | |
|
Joined: 2/27/2014 Last visit: 1/7/2026 Posts: 24 Rating:
|
Thank you! Can you upload the Light as SVG? |
| 8/27/2020 10:23 AM | |
|
Joined: 6/1/2007 Last visit: 1/12/2026 Posts: 8 Rating:
|
Is it also possible to use a svg that includes an animation? |
| 6/17/2022 8:49 AM | |
|
Posts: 64 Rating:
|
Resurrecting an old post but it seems like the best place to put this. I found the attached guide to Dynamic SVGs on the german forum and translated it to english using google translate. It's not a bad starting point to understand the format without diving into the source code. Hope it helps someone. Attachment109782045_WinCC_and_SVG_DOC_en.pdf (4318 Downloads) |
This contribution was helpful to
|
|
Follow us on