12/10/2018 1:15 PM | |
Posts: 16 Rating: (0) |
Hi, My op7 panels always goes to verify loaded data start code and then goes to the start screen. It happens once in every 20 sec. The connection to the plc seems ok. Its not displaying address not available. The MPI configured for 187.5kbps. I have programed the screen f4 for changing operating modes. in F4 K1 is set as download, K2 offline and K3 online. If i switch the op to offline mode, it doesn't restart stays with the start screen itself Could this behavior be a problem with the OP. If so why doesn't it happen in offline mode? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2018 8:13:30 AMNew subject after splitting |
|
12/11/2018 10:52 PM | |
Joined: 4/21/2015 Last visit: 5/11/2024 Posts: 53 Rating: (2) |
Connection mpi is damage.send to repair anupsrn
|
Follow us on