10/23/2021 7:12 PM | |
Joined: 5/17/2021 Last visit: 1/28/2024 Posts: 14 Rating: (0) |
I am continuing to troubleshoot an 810d based machine (CCU3/PCU20). It will not come out of estop - the estop circuit is confirmed to be working correctly, and I am able to force the I/R unit enable - something else is forcing the estop that I don't understand. I have narrowed it down (I think anyway) to DB10.DBX56.1 being set by DB8.DBX45.0 (DB10.DBX56.1 is OR'd with the estop circuit, and sets DB8.DBX56.1 if TRUE). Can any insights be gained into this failure with the diagnostic buffer? I am attaching if anyone is able to figure out what is happening. Any help would be greatly appreciated. Thanks, AttachmentDiagnose.txt (127 Downloads) |
10/28/2021 7:46 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
I guess, this is the same problem discussed under this topic. If yes follow it. |
10/28/2021 10:12 AM | |
Joined: 9/1/2005 Last visit: 5/6/2024 Posts: 4098 Rating: (193) |
closed. Please discuss the question within the thread: 810d missing files (maybe) _N_ Best regards |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on