2/16/2018 9:48 AM | |
Posts: 167 Rating: (1) |
I understand Siemens 1500 PLC support OPC UA Server (PLC act as OPC client will be released soon). https://en.wikipedia.org/wiki/OPC_Unified_Architecture
|
Last edited by: AutoGen_7361160 at: 2/16/2018 9:49:36 AMLast edited by: AutoGen_7361160 at: 2/16/2018 9:49:47 AM |
|
2/18/2018 11:22 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, Chapter 9 is all about the UA server and what you can do. |
Best regards |
|
This contribution was helpful to1 thankful Users |
3/27/2020 3:41 AM | |
Posts: 4 Rating: (0) |
Hello, I'm reviving this thread two years after its inception to ask about the support status is for the following OPC-UA features on S7 CPUs: I've been using OPC-UA methods and "Subcription" (p. 141 of s71500 communication manual, not Pub Sub) on an S7 device, and would like to use the above features. Note: I saw the recent post on MQTT support. MQTT is a supported middleware for OPC-UA PubSub. |
Last edited by: nick.james at: 03/27/2020 03:55:34Last edited by: Jen_Moderator at: 03/27/2020 10:30:25Optimized links. |
|
4/9/2020 2:02 PM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12854 Rating: (1639) |
Hello I think its not available yet. A relativly new feature is the Client functionality: https://support.industry.siemens.com/cs/de/en/view/109762770 And here you can see the supported specifications: https://support.industry.siemens.com/cs/de/en/view/109763315 An overview of the newest functions you can find here in the "new Functions " PDF https://support.industry.siemens.com/cs/de/en/view/109771626 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on