5/21/2018 2:21 PM | |
Posts: 7 Rating: (0) |
Dear all, I have tried to download the example below to see how to set up a Modbus TCP client in S7-300 PN CPU https://support.industry.siemens.com/cs/ww/en/view/109745187 For ModbusPN block it has input 'start address' and 'length', I set up as '0200' and '4' For example holding register 40200 = "11" 40201 = "22" 40202 = "33" 40203 = "44" but where do I find these data in the block?? I assume the DB instance of ModbusPN FB contains it? could anyone give me some help.. Thanks, Jason |
Last edited by: Ella0216 at: 5/21/2018 2:28:13 PMLast edited by: Jen_Moderator at: 5/22/2018 12:13:19 PMOptimized link. |
|
5/22/2018 12:16 PM | |
Joined: 6/19/2017 Last visit: 3/28/2024 Posts: 7889 Rating: (160) |
New question published by Ella0216 is split to a separate thread with the subject Need to read holding register 0010-0019 (dec) and holding register 0040-0049 (dec). Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on