(1)| 4/6/2016 10:30 AM | |
|
Posts: 16 Rating:
|
Hi, I have installed CFC v8.0+SP4, D7-SYS v8.0. I'd like to use D7-FB-Gen v2.1. But I have some issue. I created library which includes only sample block. When I tried to import library to CFC, there appeared message "Library is corrupted". Does CFC v8.0+SP4 work with library made by D7-FB-Gen v2.1? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/6/2016 11:14:23 AMNew subject after splitting |
|
| 4/6/2016 11:18 AM | |
|
Joined: 8/25/2006 Last visit: 1/15/2026 Posts: 2221 Rating:
|
Hello. Yes, it works. You need to install SP2 for D7-FB-Gen, select in the properties of D7-FB-Gen project the platform 'From D7-SYS V6.0' and recompile library. |
This contribution was helpful to
|
|
| 4/6/2016 11:40 AM | |
|
Posts: 16 Rating:
|
Thanks you, the problem is solved. |
Follow us on