(0)| 6/30/2017 3:50 PM | |
|
Joined: 9/19/2013 Last visit: 10/1/2025 Posts: 4 Rating:
|
I am working with a KP1200 Comfort Panel. Using MPI in transfer mode worked to begin the backup. The transfer gets to 91% then Prosave reports error message: The backup could not be created. I notice that using the older Simatic panels the backup file has a file format of .psb and the newer comfort panels have backup file format of .brf, does this cause any issues? Software versions? OS versions? Incompatibility issues? Maybe something in the panel memory is corrupt causing the error? Any assistance is greatly appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: rocoll at: 6/30/2017 3:52:37 PMLast edited by: Jen_Moderator at: 7/3/2017 9:32:30 AMNew subject after splitting |
|
| 11/18/2020 5:54 AM | |
|
Posts: 1 Rating:
|
Hi, Is there any solution for error while backup to USB? Thanks |
Follow us on