(0)| 5/17/2018 10:43 AM | |
|
Posts: 52 Rating:
|
hello, in your reply you recommend
what document you mean? I have third-party HMI panel (Delta Electronics) which works fine with ISO-on-TCP S7 PUT/GET for 1200 PLC, but how to setup LOGO PLC inself to enable S7 communication from 3thd-party device like this panel? We have these: Logo8 #: "6ED 1052-1MD00-0BA8", firmware 1.81.03 Should I add HMI station in LOGO project and specify TSAPs (local and remote), IP, etc. Please give an idea for this setup. BR, Yevhen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/17/2018 12:17:45 PMNew subject after splitting |
|
| 5/17/2018 10:59 AM | |
|
Joined: 12/18/2014 Last visit: 1/2/2026 Posts: 36395 Rating:
|
I mean nothing ... The statement is not from me, it is a quote from the manual and refers to the MODBUS protocol. AttachmentLOGO! 8 manual 0BA8 2016_07 (FS4) page 4.pdf (968 Downloads) |
| 5/24/2018 5:42 PM | |
|
Posts: 52 Rating:
|
Hi, I went to the application example and seemed found what I need. It is app example to connect HMI WinCC flexible - link. It should work with v7 and v8 of LOGO. I tried it with my LOGO v.8 FS04 and KTP600PN and it does not worked. I suppose the issue is with firmware FS04, (becuase really it worked with v7 of LOGO I remember that). Do you know the difference between FS versions and how they affect S7 comm. possibility of LOGO v8? |
| 7/11/2021 8:04 AM | |
|
Joined: 3/26/2019 Last visit: 1/4/2025 Posts: 5 Rating:
|
Hello Sir, Are you done with Logo plc and Delta Hmi communication. I want to do same configuration, so pl guide me. |
Follow us on