3/11/2021 12:56 PM | |
Joined: 2/10/2015 Last visit: 5/16/2025 Posts: 291 Rating:
|
hello Siemens family. I really have a serious problem. I have a new HP PC with 465 GB ssd hard drive with win 10 pro 64 bits and I have tia portal V12, 13, 14, 15,15.1 installed on the PC. I am able to open all the original projects of the machines correctly and I can go online with the PLCs without worry. But the big concern that I have is that I cannot save the different original projects after a small modification of the projects with all the versions of TIA portal that I have installed. With TIA portal v12 sp1 and v13 sp1, when I try to save the original projects after a change, I get the following error: Save the project (0025: 000045) With TIA portal v13 sp1, v14 sp1, v15.1, when want to save the original projects after a modification, I have the following error: Save project (4600: 000051) But with these same different versions of TIA portal that I installed, I manage to create new projects and I save them without problem. And even I close TIA after creation of the projects and I open them again without problem. however with the original projects of the machines, I encounter errors while wanting to save the same projects after a modification. i really need your help to find the solution to my problem. I also point out that when I was working with my old HP PC with 1TB HDD hard drive with win10 pro 64 bits, I have never encountered this kind of problem and even since I have been working in the field of automation in the past with a PC with HDD hard drive. I also point out that with SIMATIC MANAGER, SIMOTION SCOOT, WINCC FLEX2008, I do not encounter any registration problem after modifying an original project of the machines. Thank you for helping me in the emergency, good day everyone. see also attached files.
AttachmentERREUR SAVE PROJECT TIA.zip (713 Downloads) |
3/11/2021 3:59 PM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello, Have you seen this thread: https://support.industry.siemens.com/tf//ww/en/posts/project-couldn-t-save/180978?page=1&pageSize=10 Best regards, Wizard |
3/15/2021 11:31 AM | |
Joined: 2/10/2015 Last visit: 5/16/2025 Posts: 291 Rating:
|
hello sir WIZARD, I did what you advised me, but the problem still looms. I still can't save the source project after making a change. here is what i did: 1-I opened the original pojet which edited under tia v15.1 2-I made a right click on the CPU then compile then hardware (complete compilation) and then software (complete compilation). 3-I made a right click on the HMI program then compile then hardware (complete compilation) and then software (complete compilation). 4-I closed the project, I went to delete all the folders from the IM file. 5-I opened the project again then I made a right click on the CPU then compile then hardware and software (only modifications) 6- I made a right click on the HMI then compile then hardware and software (only modifications) 7-I clicked on the save project button and still the same problem. see attached files
Attachmentscreens.zip (694 Downloads) |
Follow us on