(2)| 4/19/2012 12:05 PM | |
|
Posts: 78 Rating:
|
Hi there, Can anyone assist with the connection of a PC to Masterdrive MC? I have installed the Siemens Drive Monitor software on a PC and would like to connect to the drive. The cable listed in the other posts I have produced /tf/WW/en/Posts/17310#top When I scan for the drive nothing is found? I have checked the PC Com port (Which is COM1) and matched the settings in the Siemens software to suit. I am using 9600 baud the standard speed on COM1 port. Is there anything in the drive that needs to be done to allow access? I have gone as for are possible really on my own and need a few pointers. Thanks in advance. |
This contribution was helpful to
|
|
| 4/24/2018 12:46 PM | |
|
Posts: 2 Rating:
|
Yes, i checked it. Yes i got right settings in online settings ( same bud rate in drivemonitor and in converter) |
| 4/24/2018 1:03 PM | |
|
Posts: 8092 Rating:
|
Please check the version of your DRIVEMONITER & simovert drive. |
| 4/27/2018 9:28 AM | |
|
Joined: 3/25/2008 Last visit: 1/9/2026 Posts: 230 Rating:
|
You use a physical COM1 port or a virtual one via the usb / com1 converter |
Follow us on