(0)| 11/24/2016 4:35 PM | |
|
Joined: 4/8/2016 Last visit: 12/16/2025 Posts: 133 Rating:
|
Hey Hubert, I presume you have a permission problem due to the user rights in the OS. The needed user rights for operator control of the faceplates are set in the blocks in the CFC editor. As you copied the CFC with the motor it has the same configuration as in the old project. So I would check the configuration of the authorization levels in the CFC and the user rights of the wincc user you are using. There is a Configuration Manual for the Operator Station, which should be helpful for your situation. Chapter 8 is about Setting user rights. https://support.industry.siemens.com/cs/ww/en/view/109485970 |
|
Kind regards |
|
Follow us on