10/18/2017 10:51 AM | |
Posts: 15 Rating: (0) |
Dear all, Is it possible to transmmit data from IOT2040 to HMI TP1200 comfort? Has anyone succeed in doing it? |
3/21/2018 1:54 PM | |
Joined: 1/3/2018 Last visit: 2/13/2024 Posts: 33 Rating: (0) |
Hi bergmanu, Yes, I tried with that mode the first time i tried OPC UA connection and it works. Coming back from "without security mode" to "security mode" another error occurs: "Read OPC UA connection error: Connection has been closed by client , but this transaction cannot be honored" Also I ask to the node creator Mika Karaila for certificates handling in node-red side but without success, for the moment. Corn |
3/22/2018 7:49 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, ok then it's just a certificate problem. I also asked a question on stackoverflow which is the recommended support platform for the node or the node.js package of OPC UA, not sure anymore. I hope somebody can answer our questions to solve the problem Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on